10/20/2022 8:11 PM | |
Joined: 1/14/2014 Last visit: 6/2/2024 Posts: 112 Rating: (1) |
When would this be relevant? I'm using PCS7 on a VM (Hyper-V), and my host PC acts as the license server. ALM is installed on both the host and VM, and all licenses are located on the host. I can access floating licenses without issue with the "connect to computer" option on the VM with the host saved as a favorite. However, there are some "single" licenses, i.e. OS single station and OS Runtime that are not detected by the VM. I assume this is because these need to be installed on the actual VM, due to them not being "floating" licenses. Is this correct? Would the "Check Out" transfer mode allow me to use these licenses on the VM? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/21/2022 06:52:54New subject after splitting |
|
11/4/2022 7:31 AM | |
Joined: 1/11/2019 Last visit: 10/7/2024 Posts: 764 Rating: (150)
|
Hello,
Kindly go through the attached pdf sheet in understanding the license type part. I hope it helps you! AttachmentLicense Keys.pdf (420 Downloads) |
Follow us on