1/28/2023 7:13 PM | |
Joined: 11/6/2022 Last visit: 2/5/2023 Posts: 7 Rating: (0) |
I am troubleshooting, remotely, a machines with a G120C drive.It is a very simple machine. The drive is controlled via a POT and two push buttons for direction, forward and reverse. The machine is brand new and the problem started from day one; the drive faults as soon as the forward or reverse button is pressed. Sometimes the machine works after half hour or more of trying which goes like, button press, fault, reset, recycle power, try again until it works for a while. They do not have an operator panel on the drive to read the faults. I suggested they download and install Starter. But for now, I suspect the POT is not wired correctly and would like expert opinions as to whether that may cause a problem:
Would that wiring cause a fault in the drive; by the POT supplies over or under voltage to the inputs? Thanks AttachmentDrive_Input_Terminals.pdf (344 Downloads) |
Follow us on