1/30/2023 10:23 AM | ||||||||
Joined: 3/11/2019 Last visit: 5/6/2024 Posts: 1397 Rating: (248) |
Hi RyanL99, yes the CP can be used to increase the usable connections of the CPU, but the CP can not be used to extend the max. number of total connections possible with the CPU. The CP needs an own IP-Address. The other devices must be connected to the subnet of CP. Example: The CPU 1516-3 PN/DP supports up to 256 connections in total, but only 128 via integrated interfaces. So the CP can be used if more than 128 connections are needed. But the CP can not increase the total number of max 256 connections. 6ES7516-3AN02-0AB0"
regards sancruz |
|||||||
Last edited by: sancruz at: 01/30/2023 10:29:53Feedback appreciated, please rate |
||||||||
This contribution was helpful to1 thankful Users |
Follow us on