1/24/2023 8:52 AM | |
Joined: 12/15/2016 Last visit: 3/27/2024 Posts: 2 Rating: (0) |
Hello, Can anyone help me about how can take backup from KTP 600 color DP panel? There is only MPI/PROFIBUS connection on Prosave. I am trying to connect with PC Adapter USB A2. I connected my MPI adapter with PLC and PLC connect through profibus to the HMI. My Prosave version is V16.0 I tried to make backup but it is saying message like "No connection could be established. Please verify your settings, interfaces, cables, device type etc". What will be the problem? Best Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/24/2023 11:41:18New subject after splitting |
|
1/24/2023 11:52 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
connect the adapter directly to the panel? |
1/31/2023 1:38 PM | |
Joined: 8/3/2009 Last visit: 5/10/2024 Posts: 12924 Rating: (1646)
|
Hello Pradeep_CHR the PC Adapter A2 should work with the Panel and is release for access to it: https://support.industry.siemens.com/cs/ww/en/view/19109408 -> In your screenshots we can see that your Panel has the address 0 is that correct?? the default for the Adapters and commumication processors is also 0. so check the settings of your adapter in setPGPC Interface settings in Control Panel (send a Screeenshot) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on