1/25/2023 9:52 AM | |
Joined: 4/23/2020 Last visit: 10/23/2024 Posts: 5 Rating: (0) |
Hi, I have installed Server Client arch, 5 PCs are industrial grade this pc i don't have any problem and another 3 pc has(Windows 10 Pro, 12th gen intel(R) core(TM) i5-12500T 2.00GHz, 16.0 GB RAM, 64 bit), this pc having problem while using the simatic batch recipes, so what was the error am facing means while releasing the recipes from master recipes am getting one error msg popup the popup i attached in the attachement : No connection message am getting while releasing the batch. I checked any IP Classes and PC Name classes there is no problem this 2, apart from this anything i need to check i do no any have any idea please suggest me solve this problem Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/25/2023 12:05:08New subject after splitting |
|
1/31/2023 7:01 PM | |
Joined: 4/23/2020 Last visit: 10/23/2024 Posts: 5 Rating: (0) |
Hi, No still am facing the issue. the issue not resuled |
Follow us on