1/16/2023 7:45 PM | |
Joined: 7/21/2022 Last visit: 9/17/2024 Posts: 5 Rating: (0) |
My problem is slightly different. I create HMI download files using the Card Reader/User Memory function for my projects all the time. However, my users often get messages that say the image file for the TP700 is missing. When I use TIA Portal to transfer the project it autodetects any firmware/image file differences and either upgrades or downgrades the HMI OS firmware first, before it loads my HMI project. Is it possible to put the correct image file on the USB for the HMI and have the firmware flashed when loading your project from an USB stick? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/17/2023 09:38:35New subject after splitting |
|
Follow us on