11/3/2022 7:44 PM | |
Joined: 7/25/2017 Last visit: 12/21/2023 Posts: 7 Rating: (0) |
Hello, Could you put an example of how to use copy.sh command? Do I have to use a runProgram general script and use copy.sh instead of runOkular for example? Or do I have to edit the javascript code and replace it with the command copy.sh? I tried with some options but either I get a compilation error, or it doesn't work. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/04/2022 07:47:14New subject after splitting |
|
11/3/2022 8:10 PM | |
Joined: 1/21/2013 Last visit: 6/12/2024 Posts: 2877 Rating: (460) |
Hi gustavosa, it's all described in the documentation. Here a short example: Kind regards |
This contribution was helpful to1 thankful Users |
11/4/2022 7:55 PM | |
Joined: 1/21/2013 Last visit: 6/12/2024 Posts: 2877 Rating: (460) |
Hi gustavosa,
maybe you do not use the right firmware version. You should use at least V17, Update 4. Kind regards |
Follow us on