3/15/2023 11:42 AM | |
Joined: 1/21/2013 Last visit: 10/31/2024 Posts: 3230 Rating: (501) |
Hi Pratts23, I'm not sure if you're describing a problem I would never have encountered or if you made a configuration error. When using a screen window and loading another screen within that window, the OnLoaded event of that screen is fired. Of course, the OnLoaded event of the base screen - the one that contains the screen window - does not fire, because that screen is already loaded. I have made a small example to show this. In this example, my start screen contains a screen window on the right side. Inside this window are several screens. Kind regards AttachmentLoaded_Unloaded.mpeg (319 Downloads) |
Follow us on