3/21/2023 5:43 AM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hi rikard12, I recommend using ProSave to restore the factory settings. At least this is my preferred method to do the reset or transfer another image version. And I do it several times a day. In addition to the steps described in the manual, please use 'Set PG/PC Interface (32-bit)' in the Windows Control Panel to configure the interface you are using (use the TCPIP variant) for the access point 'S7ONLINE'. Kind regards |
Follow us on