8/1/2023 10:03 AM | |
Joined: 1/21/2013 Last visit: 6/3/2024 Posts: 2830 Rating: (453)
|
Hi, I am also missing some information to understand the problem. However, I assume it is related to the Cleared event and the faceplate properties. As mentioned in the manual, the event is fired after the faceplate container is cleared. A cleared faceplate container means that the faceplate properties are no longer available. Therefore, you cannot access the faceplate properties within the event. If you are using the faceplate as a popup, you can disable the header and place a button inside your faceplate to close it. This allows you to change the property value before closing the faceplate. Kind regards |
Follow us on