10/2/2023 4:18 PM | |
Joined: 12/13/2022 Last visit: 10/18/2023 Posts: 5 Rating: (0) |
Dear Sir, Meanwhile I managed to find the issue related to the X Axis in the machine. It was the encoder that was damaged. When I was trying to check the cabling, the cabling was fine, then I had an encoder with the same characteristics from another 1FT05 motor and replaced it and everything was well. The machine started working and I only had to adjust the offset in the reference point due to having changed the encoder itself. Meanwhile, after a few days working, Now the machine is acting on me. When I start the machine, the screen starts to turn on, but after a brief moment some output lights blink and then the machine freezes, as if the PLC for some reason did not finish startup. My first thoughts were having the power not coming correctly to the CNC power supply, but it is. It is a power supply with reference 6EW 1861-3AB. It gets 220 V and I tested on the test slots for the 5 V and they are there. Do you think it might be something with the power supply? What more could I test to make sure there is nothing else? Thank you once more for your opinions and help. Best regards, Luís ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/09/2023 04:25:20New subject after splitting |
|
Follow us on