2/15/2024 1:55 PM | |
Joined: 3/13/2017 Last visit: 3/1/2024 Posts: 3 Rating: (0) |
Hi, I am currently using TIA V19. I open a faceplate from another faceplate. Is it possible to set a property from the parent faceplate to the child faceplate? The child faceplate (Drive Info) is supposed to be used by different parent faceplates (PUMP and MOTOR), where the " So when opening the Drive Info from the parent faceplate (motor or pump), I want to pass through the 'name' that comes from the parent. Is this possible? How can I do this? When using 'UI.openFaceplateInPopup', it is possible to send 'data', but when using 'Faceplate.OpenFaceplateInPopup', this seems not to be possible. ------------------------------------------------------------------------------------------ |
Last edited by: thomasTDE at: 02/15/2024 14:00:16Last edited by: thomasTDE at: 02/15/2024 14:02:20Last edited by: The Helping Hand at: 02/16/2024 09:34:27New subject after splitting |
|
2/20/2024 7:08 AM | |
Joined: 3/13/2017 Last visit: 3/1/2024 Posts: 3 Rating: (0) |
Since I don't get any response on this, I guess this is not possible. |
Follow us on