3/22/2024 10:58 AM | |
Joined: 11/10/2022 Last visit: 5/11/2024 Posts: 2 Rating: (0) |
Dear All, I need your support in creating a multimonitor WIncc Unified project. The project goes this way - 1) Currently I am have connected multiple machines from 2 different lines onto s7-1500 & Wincc unified MTP 1500 panel where I am getting the complete line performance data like production, downtimes, energy etc. 2) Now I want to share this data onto multiple 3-4 desktops where i can monitor the same data on different desktops which can be operated independently & modify PLC inputs independently on each desktop. 3) I am using TIA portal 19, I also have the option to use this on TIA 18 4) someone please suggest how to do this, I can use a unified PC runtime and share it to different monitors but I don't know how to do it as I am not much familiar with Unified PC stations Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/25/2024 08:21:44New subject after splitting |
|
Follow us on