1/11/2022 9:08 PM | |
Joined: 9/27/2006 Last visit: 8/8/2024 Posts: 12273 Rating: (2680)
|
Hello Kcanoglu; The CP 1542-5 manual suggests the use of function DPNRM_DG, which is the equivalent of SFC 13 in the Simatic Manager. Here is the link o the equipment manual (see section 5.2): https://support.industry.siemens.com/cs/ww/en/view/76894900 Here is a description of DNRM_DG from the Step 7 and WinCC v16 system manual: https://support.industry.siemens.com/cs/ww/en/view/109773506/87497403659 The following link contains a sample program of DPNRM_DG for a S7-1200 Profibus master (CM 1252-5), which you can adapt to your CP 1542-5. - "With the S7-1200, how do you read out the diagnostics data of a PROFIBUS DP slave with the "DPNRM_DG" instruction and how do you evaluate the data in the user program?" https://support.industry.siemens.com/cs/ww/en/view/66439168 Hope this helps, |
This contribution was helpful to1 thankful Users |
8/8/2024 1:03 PM | |
Joined: 7/30/2024 Last visit: 8/8/2024 Posts: 71 Rating: (1) |
New question published by Pratham001 is split to a separate thread with the subject Show Node Status on HMI. Best regards |
Follow us on