9/10/2024 10:47 AM | |
Joined: 2/17/2020 Last visit: 9/10/2024 Posts: 1053 Rating:
|
Hi, I believe you could configure your WinCC project as ServiceMode for this: SIMATIC HMI WinCC V7.5 SP2 WinCC Information System > WinCC ServiceMode WinCC ServiceMode allows you to run the WinCC Runtime project as a Windows service and access it via RDP even if the WinCC workstation has server services. However, there are also restrictions that are detailed in the manual. |
A rating will be well appreciated. |
|
Follow us on