(0)| 10/22/2024 9:26 AM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi Damla22, In this case, the first thing it would be good to know is what version of WinCC you are working with in order to try to find a solution or the reason for the problem. On the other hand, any change in computer name , user account, policies or Microsoft updates can affect the Windows user account and modify a previously working WinCC system. You can try to right-mouse click on each shortcut and choose Run As Administrator to make sure the permissions are granted in Windows to fully use the application. You can also check the Windows user to make sure it is still a member of the Administrator and Simatic HMI users group (See screenshot). Finally, I was able to find the following link to a FAQ that may help you, which is to remove the DFC from the project: "Update the configuration file of the WinCC project (delete DCF)" Best regards! Update: I forget the link |
Last edited by: ElonksuM_SN_BN at: 10/22/2024 09:27:17If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
Follow us on