7/19/2018 2:55 PM | |
Joined: 4/28/2015 Last visit: 8/7/2025 Posts: 399 Rating:
|
Hello, isn't it enough not to start the homing sequence again while the sequence is running (BUSY)...? |
7/20/2018 8:56 AM | |
Joined: 4/28/2015 Last visit: 8/7/2025 Posts: 399 Rating:
|
Hello, sorry, I do not understand your problem... With jogging, you normally do not loose the homing state of axis. So, if there is no programming problem - maybe the homing function is running - you should not loose the HomingDone bit. To reset the HomingDone bit, you have to call the function MC_Reset in mode "restart". If you do this, it is correct to loose the homing state. If there is no such problem, maybe it will be better to start a support request to check your program be the Siemens hotline... |
Follow us on