(0)| 5/23/2025 4:11 PM | |
|
Joined: 10/18/2007 Last visit: 1/15/2026 Posts: 83 Rating:
|
Update: As of yesterday, Siemens has posted an update: https://support.industry.siemens.com/cs/document/109812242/simatic-pcs-7-v9-1-sp2-software-updates?dti=0&lc=en-WW It appears the WinCC update related on May 6, 2025, which is WinCC V7.5 SP2 Upd20 is not compatible with PH. Therefore anyone with such installations should avoid installing such an update till further notice. It is frustrating and hard to believe that updates like this are coming out. In our case we now have a broken plant, which requires substantial effort to restore to a working state. Siemens, please do a much better job with your patches going forward. We have faced numerous such issues over the years, where the patch fundamentally breaks a core component of the system. |
Follow us on