(0)| 9/19/2025 2:14 PM | |
|
Joined: 3/3/2024 Last visit: 9/21/2025 Posts: 4 Rating:
|
Hi Guys Any body could help me about my CPU314C-2DP, after I configured the hardware configuration and added in the CP343-1 Lean network card, I have System Fault. I have checked hardware configuration - OK Diagnostic buffer - no fault aside from I/O writing read because i did not supply power to modules OB121 and OB122 - all inside the program block DP slavemaster - Ok address 2 Firmware version - ok Note: when I removed the program blocks OB, FC, SFC and etc SF disappeared, Now, the question is which code or what program block caused the SF fault. thanks in advance..... Ron Attachmentnetwork card preparation.pdf (13 Downloads) |
| 9/21/2025 4:03 PM | |
|
Joined: 3/3/2024 Last visit: 9/21/2025 Posts: 4 Rating:
|
Hi Daniel thanks for your answer I attached the Diagnostic buffer error information here, please help me to check. As I was told before, the errors are I/O access writing and reading as perhaps no power to supply modules during my configuration testing. I also wondering if the network card CP 343-1 Lean could work together with CPU314C-2 DP? Regards, Ron AttachmentDiagnose.txt (7 Downloads) |
| 9/21/2025 4:10 PM | |
|
Joined: 3/3/2024 Last visit: 9/21/2025 Posts: 4 Rating:
|
Hi Hati Thanks so much, I appreciate your replied. please refer to the diagnostic buffer. I believe I only have access reading writing I/O due to no power on the modules when tested but even i supplied power to all the modules I still have SF fault and the CPU unable to switch to run mode. Regards, Ron AttachmentDiagnose.txt (5 Downloads) |
Follow us on