(0)| 3/27/2025 6:36 PM | |
|
Joined: 3/27/2025 Last visit: 4/1/2025 Posts: 4 Rating:
|
ola this error has long been in the process that was old and this error in hourly time of this error or a little more or less time I could not send more photos on the same post I will send doc word so you can see doing please could help me thank you.
AttachmentET200.docx (292 Downloads) |
| 3/31/2025 3:07 PM | |
|
Joined: 3/27/2025 Last visit: 4/1/2025 Posts: 4 Rating:
|
Hello I'm forwarding the errors and photo of ET200 with said he turns off the system and is only on the output card ET200 and getting flashing the LED "RN" ET200 and then system back to work more having to be reset
AttachmentET200.docx (229 Downloads) |
| 9/22/2025 11:23 AM | |
|
Joined: 3/31/2021 Last visit: 10/23/2025 Posts: 60 Rating:
|
I have same problem,the station has an IP Address and a Device Name.Ping is working. |
Follow us on