(0)| 12/22/2025 7:58 PM | |
|
Joined: 1/21/2013 Last visit: 12/30/2025 Posts: 4372 Rating:
|
Hi Abdul, SIMATIC WinCC Unified offers many possibilities. However, the more specific your needs are, the more you will need to create a custom solution that goes beyond its features. This would require developing a custom web controls or an application based on WinCC Unified Open Pipe or the Runtime API. However, let's focus on the possibilities offered by the SIMATIC WinCC Unified system. Requirements #1 and #2 can be met using only its features. Requirement #3 can also be met, but if you have more than 32 selectable tags, you will need to address the list box limitation of only 32 elements. This can be accomplished using JavaScript-based paging. For your fourth requirement, report generation, please provide more details on what the report should look like. The SIMATIC WinCC Unified Reporting solution requires you to create an Excel template for the report. However, including tags in the template will make it difficult to meet your requirements. One way to fulfill your requirements using WinCC Unified Reporting is to create a template that contains all possible tags and then use Excel's functionality to hide the unused values. This method will require a comparably large template, which might result in poor performance. Kind regards |
Follow us on