7/28/2009 7:42 AM | |
Joined: 5/28/2008 Last visit: 6/10/2024 Posts: 4509 Rating: (837) |
Hello, 1. Why visual basic? Why you want to reinvent the wheel? Siemens offers HMI software which will be suitable for you Here's under its details:
You can see the differences between the above software in this thread. |
Last edited by: Ayman Elotaify at: 7/28/2009 7:43 AMAyman Elotaify |
|
7/28/2009 7:44 AM | |
Posts: 2930 Rating: (432)
|
Hi, Could it be possible to use visual basic 6.0 to control the input of CPU 222? No, you can only read Inputs. But you can control flags or outputs Could the S7-200 connect to the PC using RS232? Yes. You can use the RS232 PC-PPi programming cable 6ES7 901-3CB30-0XA0 Could it be possibel to use Visual Basic 6.0 to make a GUI for the project? Download the PC-Access Demo here: https://www.automation.siemens.com/_en/s7-200/support/tools_downloads/pcaccess.html This is a 60 day license wihtout limitation. I do not know if VB V6.0 is supported. Could you give me a sample program using Visual Basic 6.0 communicating with the PLC? See the examples comming with PC-Access. I hope this helps |
8/5/2009 9:54 AM | |
Posts: 3 Rating: (0) |
|
Last edited by: sinjid at: 8/5/2009 9:58 AM |
|
Follow us on