10/16/2009 4:04 PM | |
Joined: 9/27/2006 Last visit: 5/3/2024 Posts: 12257 Rating: (2666) |
Hello Sidou; S5 timers exist in almost the same format in Step 7. As described in the S5 to S7 converter manual: (see table 3-12) http://support.automation.siemens.com/WW/view/en/1118413 Instruction Type S5 S7 Timer instructions SP, SE, SD, SP, SE, SD, SS/SSU, SF/SFD,SS, SF FR, SEC FR, S T Appendix A of the same manual will show the instruction list comparison between S5 nd S7, and the online help of Step 7 will give you all details of each timer instruction. |
Last edited by: dchartier at: 10/16/2009 4:05 PM |
|
10/16/2009 9:51 PM | |
Posts: 15 Rating: (0) |
yes that's write I WOULD YOU TO SHOW ME THE SHAPE OF SD timer in step5 and how it is in step7 programming with logic mode not list. thanks |
10/16/2009 10:15 PM | |
Posts: 15 Rating: (0) |
WHICH ONE OF THESE TIMERS IS SD TYPE IN STEP5 |
Follow us on