11/18/2009 8:34 AM | |
Posts: 77 Rating: (0) |
Dear all, I found OB 20 in my CPU 103 program. But based on what i have read, CPU 103 doesn't have OB 20. CPU 103 only have OB 1, OB 2, OB 13, OB 21, OB 22, OB 34, OB 31 and OB 251. Why OB 20 can be found in CPU 103? Then I found OB 21 in my program, if i want to convert it to S7-300(customer request) where should i convert it to? OB 100 or OB 101? And for OB 20, it should be convert to OB 100 isn't it? hereby i enclosed the program. Thank you all, AttachmentBA_FF@ST.zip (100 Downloads) |
11/19/2009 10:50 AM | |
Posts: 77 Rating: (0) |
Sorry, I can't check it in online right now. And then for OB20, I think I'm just deleting it right?? Is it okay?? Thank you |
11/20/2009 2:48 AM | |
Posts: 77 Rating: (0) |
Yes sir, Thank you for the answer |
Follow us on