Industry Online Support
Technical Forum
8/11/2010 7:48 PM | |
Joined: 4/10/2008 Last visit: 12/29/2023 Posts: 4 Rating: (0) |
Hello, I have a HMI Coros OP35 and need to exchange it for an HMI Coros OP37. PROBLEMS. - Communication is via PROFIBUS-DP via an IM-308B. -I can not found a file (*. 200) for HMI Coros OP37.On thissite(from siemens),HMI Coros OP37,is not in the list.Does this HMI is supported by the IM-308B? - the list shows "SI8020TD.200 Coros TD / OP". This file is for all OP and TD?
|
8/12/2010 10:53 AM | |
Joined: 10/7/2005 Last visit: 5/27/2024 Posts: 3007 Rating: (1049)
|
Hello DELByXARK The COROS OP37 should be ok on an IM308B (revision A6 or later) according to the link below: Configurable HMI devices as DP slaves for connecting to the IM 308B (A6) I am reasonably sure that the generic "Coros TD/OP" typefile is applicable for all the COROS OP's inCOM ET200, but am not 100% certain on this one. Perhaps others can confirm this, but if not I suggest you send an enquiry straight to the guys from ComDeCwho I found to be very helpful and knowledgeable in the past concerning all things COM ET200 typefile related. |
Cheers |
|
Follow us on