3/4/2011 2:14 PM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating:
|
Hello dear colleagues. I will try to explain my problem as best as i can. I have a project in wichi have used severalPLC's and each PLC contains severalS7 Graph sequencers,because i just copied and pasted the Graph sequencers froma"X" PLC to other (to save time because the sequencers are simillar eachother) i just corrupt the proagent diagnostics of the complete project (before this i did not know the right way to export S7 Graph sequencers by means of the source generation tool). Now i have to rebuild my complete project from 0% (to be honest i have already done it with other 2 projects before this), but in this project i'm having some problems to generate the source files for S7 Graph sequencers. AttachmentFB180_SOURCE.zip (411 Downloads) |
Last edited by: TEBANCH at: 3/7/2011 1:29 PMInformation update! Keep working! |
|
3/11/2011 3:28 PM | |
Joined: 10/7/2005 Last visit: 9/10/2025 Posts: 3049 Rating:
|
Hello TEBANCH not too sure how much this going to help you, but your source file opens up ok for me (I tried both ways, insert as "External Source" and open it as well as insert a"Graph Source" and then openthe source file from it). The only problem I have is that the used addresses are unknown which is expected though (I don't have the DB's nor teh symbolic declaration for the used I/Q/M bits in it). Attached is a screen dump of what I'm getting and my software versions are Step 7 V5.5 & S7 Graph V5.3 SP6. Have you tried to open it with a different PC (perhaps something is wrong with your Step 7 or Graph version)? |
Cheers |
|
3/12/2011 1:44 AM | |
Joined: 10/7/2005 Last visit: 9/10/2025 Posts: 3049 Rating:
|
Hello TEBANCH it could very well be a version conflict (it wouldn't hurt to get both S7 Graph versions up to the same version and SP). Questions: 1.) Does the graph source fiel opens ok in a new S7 project on the same PC on which it was created? 2.) Have you tried to do a source file export with address priority instead of symbol priority (go to "Options" -> "Application settings" in S7Graph to change this) 3.) As you current S7 Graph source file is symbol based, do you have all the symbolic entries in your symbol table? (I initially got an "the symbolic name is incorrect" error when trying to open the source and had to add FB180 with symbolic name "FBControlStop" to the symol table).. I hope this helps and let us know what you find out. |
Cheers |
|
Follow us on