6/12/2011 8:44 AM | |
Posts: 691 Rating: (36) |
You can use SFC 14 and SFC 15 ( DP_RD and DP_WR) for reading the Profibus Devices |
6/12/2011 2:59 PM | |
Joined: 10/7/2005 Last visit: 6/2/2024 Posts: 3007 Rating: (1049) |
Hello Pranab a quick and easy search at https://support.automation.siemens.comreveals the following which I hope will help: Micromaster 4 -- Commissioning and operation -- Using PROFIBUS DP Sinamics G120 -- Commissioning and operation -- Using PROFIBUS DP SINAMICS G120, MICROMASTER 4: Acyclic reading and writing parameters of the frequency inverters via PROFINET and PROFIBUS @ Saravana kumar: A Sinamics Drive can most certainly be a Profibus slaves (what makes you think it can't), |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on