6/23/2011 11:22 AM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
Hello Dolf PLCSIM supports only the SFB versions of GET and PUT (which are used in S7-400's) but NOT the FB versions (which are used in S7-300's and "wrap" extra code around the GET/PUT SFB's). As PLCSIM does NOT know (nor care) that you use S7-300's, the only way to simulate the comms in your case is to replace the FB 14/15 with SFB14/15 calls in your program and more can be foundat the link below: How do you simulate communication between two CPU modules? I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on