12/1/2006 12:01 AM | |
Posts: 27 Rating: (0) |
|
12/2/2006 4:51 AM | |
Joined: 8/24/2006 Last visit: 3/20/2024 Posts: 20 Rating: (2) |
Dear Draxelmaier I have enclosed the bitmap image of FC106. In this image the MD20 is of the data type Real. The value required for this is to be generated by your logic. And the Upper limit in my example is say 100Kg and the lower limit is 0Kg. So depending on the value of the MD20 (i.e between 0 to 100Kg) the value of the PQW(Analog output) is varied between 0 to 10 V. I am not able to understand your application using tension etc.. Hence I have explained with and example of Kg-Weight. Sandoz[:)] |
Follow us on