6/29/2011 5:50 PM | |
Posts: 23 Rating:
|
Dear All, Iam using FM 355 C PID controller in my project to control the pressure control valve in the inlet and in the discharge line I have presssue transmitter with 0-275 psi range. I have manual / auto selection from scada. If the controller is off the external manipulated output istransfered from scada to the PID.When the controller is on then the PID should control but in my case the problem is when i change it to auto there is no PID action no matter what P and I value i set in the range P = 0.2 to 2.5 I= 10 to 60 s D=0 Tried with different setpoint 35, 30, 35, 40, 45 & 50 psi but when i switch on the controller it starts opening/closing the valve in forward or reverse direction from the previous manual output for eg ( 30 % PCV open ). Kindly suggest any additional parameters i need to set apart from MOD_ADD, CHANNEL, COM_RST, LOAD_PAR, SP_RE, LMN_RE, LMN_REON, SP_HLM, SP_LLM, GAIN, TI, TD, LMN_HLM, LMN_LLM. Thanks. AttachmentPID_Snaps.zip (291 Downloads) |
6/29/2011 10:56 PM | |
Joined: 1/28/2009 Last visit: 9/15/2025 Posts: 6875 Rating:
|
Hi Check if the machine (Such as a compressor) not operating in the unsafe region of operation for a short time?Some safety i ssues which is considered in the loop design may cause that. Check the process conditions and track the curves and logic to undrestand the cause of emergency action of the valve. //check the attachment Regards Attachment2.zip (302 Downloads) |
Follow us on