7/21/2011 10:41 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hi, Have a look on the following Link also before Upgradation. Software update with utilization of new functions (PCS 7 V6.x or higher to V7.1) Software update without utilization of new functions (PCS 7 V6.x or higher to V7.1) |
Ammy |
|
7/21/2011 11:03 AM | |
Posts: 836 Rating: (100) |
Hi, as my predecessors already said it is ok to upgrade the software. You hardware matches the system requirements of PCS 7 7.1. Refer to this entry for description of upgrade process: http://support.automation.siemens.com/WW/view/en/39980937 |
This contribution was helpful to1 thankful Users |
7/23/2011 12:52 AM | |
Posts: 88 Rating: (0) |
Dear Mr. TAGOLOVER... kindly explain the procedure of upgradation from 6.1+sp2 to 7.1+sp1 or sp3 |
Follow us on