10/20/2011 2:04 PM | |
Posts: 557 Rating: (64) |
hi Can we use distributed I/O module in profinet with below module. CP 343-1 Advanced(6GK7 343-1GX30-OXE0) Regards |
10/21/2011 7:51 AM | |
Posts: 557 Rating: (64) |
Hi, I am not getting profinet line in hardware configuration. Is there any setting to configure distributed i/o on profinet. Regards |
10/21/2011 9:57 AM | |
Joined: 10/7/2005 Last visit: 6/10/2024 Posts: 3008 Rating: (1051)
|
Hello Eastern right click on the"PN-IO" port of the CP343,select "insert PROFINET IO System" and your line should (hopefully will) appear. Note that you'll need to use PNIO_SEND (FC11) and PNIO_RECV (FC12) as per message box that will pop up when you insert the PROFINET IO System. I hope this helps |
Cheers |
|
Follow us on