12/6/2011 4:40 PM | |
Joined: 7/27/2009 Last visit: 2/13/2025 Posts: 36 Rating:
|
Hi, Thank you for the quick reply. First of all, I am sure enough that this is not a licence problem: I have a licence for Step 7 Professional V11. Here are more information in regard to the scenario: a. First of all I created a new, empty project. I added an unspeciffied CPU 1200 and clicked on Detect so that the HW configuration is mirrored. (this worked like a charm) b. Right click on the PLC_1 Device and select Compare > Offline/Online The Info tab/ General displays the error depicted in image1.jpg The block list displays the denied sign depicted in image2.jpg Double click on the block displays the error in image3.jpg Thank you Attachmentimages.zip (845 Downloads) |
Follow us on