1/4/2012 5:39 PM | |
Posts: 14 Rating: (0) |
Hello all, After upgrading from Step 7 V5.4 to V5.5, I am now having issues with a couple of projects where the PLC 314C-2DP (integrated into a Sinumerik NCU 571.4 6FC5357-0BB14-0AA0) is not being recognized, and therefore nothing shows up in the project. I do not have, and never have had the 840D package installed. The previous version V5.4 did make note of some hardware mismatch with the hardware catalog (see attachments below), but this did not impede the use of the project for online troubleshooting with the PLC. I have tried udating the hardware catalog via internet and by downloading the hardware updates but while the catalog is updated, the issue remains unchanged. Any suggestions, known issues with this PLC and the V5.5 software? Thanks Attachment314c2DP.zip (147 Downloads) |
1/5/2012 4:56 AM | |
Posts: 2964 Rating: (481)
|
Hello.... AttachmentPLC314C_DP.pdf (188 Downloads) |
Follow us on