(0)| 10/11/2012 6:16 AM | |
|
Posts: 461 Rating:
|
Hi , As i was trying to perform the datalog sample program of Pegaia ,I was not able to download the program with memory card present in in the cpu1212c.Once removed i was able to download. Memory Card - Siemens card 256 MB. I am getting an hardware Configuration error, i attached the error img iam getting. I dont know whether to configure any setting to use memory card.. Also i tried a simple project without program except main & while trying with memory card i getting the same Hardware configuration error. I made a CPU reset removing the MC & then after downloading the code cpu was in stop mode at that instant i inserted the MC then the cpu's MAINT stated to Blink in yellow. Please guide me go to next step in datalogging. Thanks & Regards, Nelliyan.G |
Last edited by: Nelliyan randy at: 10/11/2012 8:48 AMLast edited by: Nelliyan randy at: 10/11/2012 8:44 AM |
|
| 10/26/2012 5:29 PM | |
|
Posts: 28 Rating:
|
Hi Nelliyan, I'm not sureif a 256 MB card will work with a 1200 series CPU. The S7-1200 system manual states that program cards are either 2, 12, or 24 MB SD cards. I found a post that may pose the same problem: /tf/WW/en/Posts/75317 I know it doesn't really solve anything, but I would definitely check first to see if your card is compatible. Best wishes, Cyrus |
This contribution was helpful to
|
|
Follow us on