6/18/2013 10:41 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello ryan3, If you only have the two plc, have you closed the terminating resistors? |
6/18/2013 11:10 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (713) |
Hello, And check the arrows on the profibus connector too. Here you will find an example follow the steps carefully and it must work. D6 - PROFIBUS DP with Master CPU 315-2 DP / Slave CPU 315-2DPJust change the CPU. Regards, Marcjan |
Problem solved? |
|
6/19/2013 2:48 AM | |
Joined: 11/9/2009 Last visit: 5/1/2024 Posts: 41 Rating: (0) |
but sr im sorry i have only these 2 plc it is possible or will work? |
6/19/2013 2:48 AM | |
Joined: 11/9/2009 Last visit: 5/1/2024 Posts: 41 Rating: (0) |
yes sr.i closed the resistor. |
Last edited by: ryan3 at: 6/19/2013 2:49 AM |
|
Follow us on