Industry Online Support
Technical Forum
9/9/2013 12:06 PM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of the User HRAY
|
9/9/2013 12:32 PM | |
Joined: 4/24/2006 Last visit: 10/18/2024 Posts: 8746 Rating: (1169) |
Hello, You need to use a DP/DP Coupler. Best regards, Wizard |
9/9/2013 9:02 PM | |
Joined: 8/18/2011 Last visit: 9/9/2022 Posts: 14 Rating: (0) |
Dear Sir. Wizard, You can give me sample program for that?.. thanks..
|
9/9/2013 10:25 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello HRSAY; There is no programming to do, except to read and write to the addresses given in the DP/DP couplert. See the first section of the following FAQ: What are the special features of input/output addressing with the DP/DP coupler? Hope this helps, Daniel Chartier |
Follow us on