Industry Online Support
Technical Forum
9/29/2013 1:55 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, What the printer needs is an array of bytes, some of them being ascii coded (your label for instance) other being hex coded (the escape command). You can prepare an array of bytes/char and move what you need in that array before sending the array to the printer. In the instruction set, in the folder "extenbded instructions ==> String + Char" you will find instructions like: - Strg_TO_Chars: this instruction copies characters from a character string STRING to a field of several characters of the data type CHAR or BYTE (Array of CHAR / BYTE). In annex a small example trying to explain the idea. FC1 is written in SCL FC2 is written in LAD But both do the same thing. Placing the sequence "escapeA" in front of a label string as buffer to be sent to the printer. AttachmentProgram blocks.pdf (227 Downloads) |
Best regards |
|
This contribution was helpful to
1 thankful Users |
Follow us on