(0)| 1/16/2014 3:07 PM | |
|
Posts: 13 Rating:
|
Hi Is it somehow possible to change the value "On threshold" in an "Up/down counter" via an analog input (0-10V)?
|
| 1/18/2014 8:29 PM | |
|
Joined: 12/27/2006 Last visit: 11/17/2025 Posts: 1200 Rating:
|
Yes thats possible, only if you use a LOGO 0BA6 or 0BA7 Look in the attachment And.. You can use Di7 as Analog input and Di8 as digital input. Even, if you can programm, u can use a single inpu zb Di 7 as a analog inout and as a digtal input. Then you have to make a sort of multiplexing Look in the attachment In the second part of the sceme ther is a kind of multiplexing AttachmentAnalog_tresholt.zip (312 Downloads) |
| 2/4/2014 8:04 AM | |
|
Posts: 340 Rating:
|
new question is splittet to isn't it possible to use only one of the LOGO! V6 digital inputs as an analog input? |
Follow us on