5/15/2014 9:58 PM | |
Joined: 6/18/2008 Last visit: 3/3/2024 Posts: 108 Rating:
|
I'm really confused. I explain the problem again. While reversing archieve file,i unchecked "Stop with end transmission sign" the system restored the files until _P_0E00015P( FB15 ) but at _P_0E00015P files,it restored some part of file and at error log, it showed error data. It is noticeable that NCU(6FC5357-0BA10-0AE0 , NCU 571.2) card and PC card are very old and i havenot been succeed to get them so far. As i mentioned, there were 2 VMC machines. One of them worked ok an the other one didn't. When i put the PCMCIA card of out of worke machine on the ok one, both of them were defected. their problems are as follow: Why does H3(7-Segment in NCU) act unnormal,when NCU is starting up? H3 shows number 7 and after a while(about 10 seconds) it shows 3 and finally number 6. I got PLC program but i don't know By what version of simatic manager software it can be opened? It wasn't opened by simatic manager V5.4 and STEP 7 Lite V3.0 The program is attached. I'm waiting hopefully for your help. Thnaks.
AttachmentPLC_PCMCIA.zip (183 Downloads) |
Follow us on