Industry Online Support
Technical Forum
9/7/2014 6:43 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
The batteries, which you are using, are those of same capacity? Are those from Siemens or are from local market? |
9/7/2014 7:43 AM | |
Joined: 9/4/2014 Last visit: 5/3/2022 Posts: 3 Rating: (0) |
they are of Varta with the same voltage and amperage |
9/7/2014 12:21 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
I strongly recomend to use battery from Siemens only& check the life, instead of conducting any expriments. |
9/7/2014 12:42 PM | |
Joined: 9/4/2014 Last visit: 5/3/2022 Posts: 3 Rating: (0) |
thank you very much, unfortunately I could not find the original |
Follow us on