10/7/2014 5:45 PM | |
Posts: 20 Rating: (4) |
Dear all, I have a Field PG M4 (6ES7716-2DA11-0CB3) with CORE I7-3520M, Intel HD4000 graphics, Windows 7. I would like to use an external display with this PG whenI am working in the office. The manual states that the DPP display port can output to a monitor with a resolution of 2560 x 1600. Does anyone know if it is possible to run an additional monitor at 2560 x 1600 as an extended desktop, with the PG built in display at the maximum of 1920 x 1080? I don't want to buy an expensive 2560 x 1600 monitor if it will not work with my PG. |
Follow us on