(0)| 1/25/2008 8:02 PM | |
|
Posts: 297 Rating:
|
It depends on what you want to do with the USB stick. If you are at a high enough password level, you can use the DOS SHELL function in Startup under MMC. You can either use dos commands or start Explorer. If you want to use the Services area with Data In or Data Out, I know of 2 methods. First is to buy and install the DNC Machine option. You can assign a soft key to the G drive. The other method is to replace the function of the Disk/Card button with the G drive. If you do this, you cannot access the floppy any more. See http://support.automation.siemens.com/WW/view/en/27106861for an example. While this is written for SinuTrain, it does work on an 840D. You may have to replace the keyword [Services] with [Dienste]. Hope this helps. SteveA |
Follow us on