1/15/2013 4:35 PM | |
Joined: 2/20/2012 Last visit: 5/11/2023 Posts: 62 Rating:
|
Hi All, I am facing a new problem when I am trying to compile the OS in my PCS 7 project. The error is as follows in the log: Internal Error: Compilation of Process variables was aborted. Error number :15124 In the compilation dialog box, the error no. it gives is "302:3000". How do I get to know what is the error? Attached is the log of the compilation. Please let me know your advices on how to take out this error. Thanks, Sudheendra
AttachmentTRANSFER.pdf (749 Downloads) |
1/15/2013 6:39 PM | |
Posts: 2661 Rating:
|
Hi Sudheendra R, The error you are getting seems similar to the one described in the following FAQ: How do you clear the error message "Internal error: transfer of process variables has been aborted. Error number: 15424" when compiling the OS project? Also make sure there are no"extra" client licenses on the ES. Regards |
Follow us on