1/4/2016 3:43 PM | |
Posts: 3 Rating: (0) |
Dear Forum Users, Our company recently bought a CNC Grinding machine. While we were recommissioning the machine, we were able to jog the cnc axis but somehow after a while we were not able to do that. A few people were working on the machine simultaneously so we are not able to detect what caused the problem. However as mentioned on the forum I have checked 63 -64-48-663-112. Could not find 65. All are giving 24V signal. I have a 840D controller and 611 drive module. On checking DB31.DBX2.1 result is Zero DB31.DBX21.7 is 1 DB31.DBX1.5 is 1 DB31.DBX1.7 is 1 DB31.DBX4.3 is zero. This case is with all axis. Timer T32 is zero. Please suggest a possible solution. Regards Aman AttachmentIMG_20160104_150238[1].jpg.pdf (643 Downloads) |
Follow us on