4/8/2016 9:07 PM | |
Joined: 9/27/2006 Last visit: 11/11/2024 Posts: 12293 Rating: (2691) |
Hello erk; Do you have the multi-VGA card option for WinCC v6? I believe it is required for that version. If yes, follow the instructions in this FAQ: Display of oversize process pictures spread over several monitors https://support.industry.siemens.com/cs/ww/en/view/13287608 If not, you can do it manually (with a bit more work of course): start by detecting/activating both monitors through the Windows OS Control Panel. Then in WinCC create a single PDL with a double resolution (enough to cover both monitors). I would then create 2 picture windows inside this PDL dividing the screen in 2 (each one for one monitor) and showing a different view of your project in each. See the following discussion for hints: Dual monitor in WINCC v6.0 https://support.industry.siemens.com/tf/ww/en/posts/4351/ Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/9/2016 11:33:14 PM |
|
4/9/2016 11:34 PM | |
Joined: 9/27/2006 Last visit: 11/11/2024 Posts: 12293 Rating: (2691) |
|
This contribution was helpful to1 thankful Users |
Follow us on