4/12/2016 11:00 AM | |
Posts: 18 Rating:
|
The CU unit is sinumerik 802D sl T/M pro Version D Software is 01.04.01.07 is this sufficient? Line module is attached. |
4/12/2016 1:09 PM | |
Posts: 18 Rating:
|
There is no info on either left or right side of the sinamic drive unit. is there anywhere else i can check? |
4/12/2016 1:13 PM | |
Posts: 18 Rating:
|
this is the front of electric diagram from the machine if it helps? |
4/12/2016 1:47 PM |
|
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
I am studying the same & shall come back. |
4/13/2016 7:29 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, I am afraid with present X20 or X21 connector touch probe could not be interfaced. The best option would be go for MCPA interface module. Interface & configure its DI/DO for touch probe parametrs. PLC program & parameter setting needs to be carried out & by this way touch probe could be bought into operation. Please refer manual table 1.1 page 19, chapter 2.2, 5.4, 5.6, 8.5 & 8.6 for the same. HTH. |
Last edited by: PISCEAN 2010 at: 4/13/2016 7:31:01 AM |
|
Follow us on