(0)| 7/8/2016 2:33 AM | |
|
Posts: 7 Rating:
|
Hello! I have 2 identical device set on the one profibus line. Sentron PAC 7KM2112-0BA00-3AA0 | SW-REV: v2.2.2 | BL-REV: v1.0.2 | + Profibus module 7KM9300-0AB00-0AA0 | FW: v3.0.3. I have installed SI018163.gsd and SIEM8163.gsd from thispage. First one is OK. But second one is not available. Both device set have identical HW configuration (apart DP address). DP addreses are unique. Communication status of 'bad' module - DIAG:WAIT_PRM. Update#1: I can see both PAC3200 when I use transmission rate 500 Kbps, but I need 1.5 Mbps. Update#2: I have updated frimware on 'bad' PAC3200 2.2.2 ->2.4.1. There are no changes. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Pavel_Promatis at: 7/8/2016 8:00:20 AMLast edited by: Min_Moderator at: 7/8/2016 12:18:00 PMNew subject after splitting Last edited by: Pavel_Promatis at: 7/11/2016 10:58:23 AM |
|
Follow us on