7/12/2016 10:08 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi, MAC-Adress have to be different. see the Wikipedia entry about it. As I remember it is possible to load an other MAC adress to the modules. There is no need to change it, but I would change it in the project and load the configuration in CP. When the MLFB/order no. and the FW are the same you don´t have to change anything else in HW-config. regards, |
Last edited by: mopS04 at: 7/12/2016 10:14:24 AMFCK WAR! |
|
7/18/2016 1:24 PM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
Dearvakarthik88, As per your first post, you have 2 numbers of CP443 in each rack. So total of 2+2=4 CP443. In one , none of the LED are on. You can swap this CP with Red Rack's CP and confirm is it problem with module or back plane easily. Dear Mops04, Is there any easy way to check back--plane voltage using multi-meter? (between any pins? ) |
Last edited by: vipz at: 7/18/2016 1:25:39 PM
|
|
Follow us on