1/9/2017 7:33 PM | |
Posts: 1 Rating: (0) |
We have a large vertical turning center with full c-axis contouring. Two alarms are coming up: Axis C1 hardware fault of active encoder and Axis SP11 hardware fault of active encoder. We have had contamination in the C axis rotary encoder in the past. That gave us a different alarm. I also know from past experience that the table and all axis will allow me to move the axes in all axis. At least in turning mode. I have also removed the rotary encoder from the chuck (Conected electronically) in the past while doing maintenance on the machine, I was still able to move the axes and use MDA (MDI) to comand the machine. This alarm combination will not allow me to go into MDA (MDI) or jog the machine. I am aloso seeking answers from thw hotline and the manufacture. Thanks, Sam ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/10/2017 12:03:17 PMNew subject after splitting |
|
Follow us on